:STATus:LLINE:EVENt?

Instrument:
N1010A
N1000A
DCA-M
Meas. mode:
Scope
Eye
Jitter
TDR
Flex Apps:
FlexDCA
FlexRT

Query Syntax

:STATus:LLINE:EVENt?

Description

Reads the limit line event register to determine the status of individual status bits. The decimal-weighted value of the register is returned. The only bit used is bit 0 (COMP), which indicated if a limit-line-based limit test has completed. Reporting of event register bits in the status register system is controlled by the mask loaded into the enable register. All true event bits, that are enabled, are logically OR'ed, which results in setting true bit 5 (LLINE) of the Operation Status Register. Use the :LLINe subsystem to configure a limit-line-based limit test.

Limit Line Register Commands
Register Read Write Command
Event ♦   :STATus:LLINE:EVENt?
Enable (mask) ♦ ♦ :STATus:LLINE:ENABle
Limit Line Status Registers
Bit 7 6 5 4 3 2 1 0
Bit
Weight
128 64 32 16 8 4 2 1
Event
Register
— — — — — — — COMP
Enable
Register
               
Sets to Bit 5 (LLINE) of Operation Status Register

Bit Definitions

COMP
A true indicates that a limit-line test has completed.