:STATus:CRECovery:ENABle

Instrument:
N1010A
N1000A
DCA-M
Meas. mode:
Scope
Eye
Jitter
TDR
Flex Apps:
FlexDCA
FlexRT
FlexPLL

Command Syntax

:STATus:CRECovery:ENABle <mask>

<mask> is an integer, 0 to 255, representing a mask for the bits in the event register.

Query Syntax

:STATus:CRECovery:ENABle?

Description

Enters a decimal-weighted value in the clock recovery enable register that masks the ability to report bits in the clock recovery event register.

Clock Recovery Register Commands
Register Read Write Command
Event ♦   :STATus:CRECovery:EVENt?
Enable (mask) ♦ ♦ :STATus:CRECovery:ENABle
Clock Recovery Status Registers
Bit 7 6 5 4 3 2 1 0
Bit
Weight
128 64 32 16 8 4 2 1
Event
Register
— LKFIN LKSTRT — — — LOCK UNLK
Enable
Register
               
Sets to Bit 7 (CLCK) of Operation Status Register

Bit Definitions

UNLK
True indicates that clock recovery is unlocked. This occurs when an 83491/2/3/4/5/6A Clock Recovery module or and 86108A/B Precision Waveform Analyzer module or an N1060A Precision Waveform Analyzer module becomes unlocked or trigger loss has occurred. If an 83496A module is locked, sending the :CRECovery:RELock command does not set the UNLK or LOCK bits. To determine if the RELock command has completed, use the :CRECovery:LOCKed?.
LOCK
True indicates that clock recovery is locked or a trigger capture has occurred.
LKSTRT
True indicates that the clock recovery re-lock routine has started.
LKFIN
True indicates that the clock recovery re-lock routine has finished.