:STATus:USER:ENABle

Instrument:
N1010A
N1000A
DCA-M
Meas. mode:
Scope
Eye
Jitter
TDR
Flex Apps:
FlexDCA
FlexRT
FlexPLL

Command Syntax

:STATus:USER:ENABle <mask>

<mask> is an integer, 0 to 255, representing a mask for the bits in the event register.

Query Syntax

:STATus:USER:ENABle?

Description

Enters a decimal-weighted value in the user enable register that masks the ability to report bits in the user event register.

User Register Commands
Register Read Write Command
Event ♦   :STATus:USER:EVENt?
Enable (mask) ♦ ♦ :STATus:USER:ENABle
User Status Registers
Bit 7 6 5 4 3 2 1 0
Bit
Weight
128 64 32 16 8 4 2 1
Event
Register
— — — SLOT4 SLOT2 SLOT3 SLOT1 LCL
Enable
Register
               
Sets to Bit 1 (USR) of Status Byte Register

Bit Definitions

LCL
A true indicates that FlexDCA has transitioned from remote mode to local mode. This status bit originates from the local event register.
SLOT1
Reserved for future use.
SLOT3
Reserved for future use.
SLOT2
Reserved for future use.
SLOT4
Reserved for future use.