:STATus:MESSage:EVENt?

Instrument:
N1010A
N1000A
DCA-M
Meas. mode:
Scope
Eye
Jitter
TDR
Flex Apps:
FlexDCA
FlexRT
FlexPLL

Query Syntax

:STATus:MESSage:EVENt?

Description

Reads the message event register to determine the status of individual status bits. The decimal-weighted value of the register is returned. The only bit used is bit 0 (MSG), which indicates if a message is displayed on FlexDCA's screen and placed in the message queue. Reporting of event register bits in the status register system is controlled by the mask loaded into the enable register. All true event bits, that are enabled, are logically OR'ed, which results in setting true bit 2 (MSG) of the Status Byte Register.

Message Register Commands
Register Read Write Command
Event ♦   :STATus:MESSage:EVENt?
Enable (mask) ♦ ♦ :STATus:MESSage:ENABle
Message Status Registers
Bit 7 6 5 4 3 2 1 0
Bit
Weight
128 64 32 16 8 4 2 1
Event
Register
— — — — — — — MSG
Enable
Register
               
Sets to Bit 2 (MSG) of Status Byte Register

Bit Definitions

MSG
A true indicates that a message is displayed on FlexDCA's screen and placed in the message queue.