:STATus:JITTer:EVENt?

Instrument:
N1010A
N1000A
DCA-M
Meas. mode:
Scope
Eye
Jitter
TDR
Flex Apps:
FlexDCA
FlexRT

Query Syntax

:STATus:JITTer:EVENt?

Description

Reads the jitter event register to determine the status of individual status bits. The decimal-weighted value of the register is returned. Reporting of event register bits in the status register system is controlled by the mask loaded into the enable register. All true event bits, that are enabled, are logically OR'ed, which results in setting true bit 9 (ACQ) of the Operation Status Register.

Jitter Register Commands
Register Read Write Command
Event ♦   :STATus:JITTer:EVENt?
Enable (mask) ♦ ♦ :STATus:JITTer:ENABle
Jitter Status Registers
Bit 7 6 5 4 3 2 1 0
Bit
Weight
128 64 32 16 8 4 2 1
Event
Register
— — — — — AREQD JLOSS —
Enable
Register
               
Sets to Bit 12 (JIT) of Operation Status Register

Bit Definitions

JLOSS
A true indicates that the pattern synchronization is lost in Jitter Mode.
AREQD
A true indicates that a parameter change in Jitter Mode has made an Auto Scale necessary.