:STATus:LTESt:EVENt?

Instrument:
N1010A
N1000A
DCA-M
Meas. mode:
Scope
Eye
Jitter
TDR
Flex Apps:
FlexDCA
FlexRT

Query Syntax

:STATus:LTESt:EVENt?

Description

Reads the limit test event register to determine the status of individual status bits. The decimal-weighted value of the register is returned. The only bit used is bit 0 (COMP), which indicated if a limit test has completed. Reporting of event register bits in the status register system is controlled by the mask loaded into the enable register. All true event bits, that are enabled, are logically OR'ed, which results in setting true bit 8 (LTEST) of the Operation Status Register. Use the :LTESt subsystem to configure a limit test. The limit test event register is used only when a measurement limit test completes.

Limit Test Register Commands
Register Read Write Command
Event ♦   :STATus:LTESt:EVENt?
Enable (mask) ♦ ♦ :STATus:LTESt:ENABle
Limit Test Status Registers
Bit 7 6 5 4 3 2 1 0
Bit
Weight
128 64 32 16 8 4 2 1
Event
Register
— — — — — — — COMP
Enable
Register
               
Sets to Bit 8 (LTEST) of Operation Status Register

Bit Definitions

COMP
A true indicates that a limit test has completed.