:STATus:PTIMebase:EVENt?

Instrument:
N1010A
N1000A
DCA-M
Meas. mode:
Scope
Eye
Jitter
TDR
Flex Apps:
FlexDCA
FlexRT

Query Syntax

:STATus:PTIMebase:EVENt?

Description

Reads the precision timebase event register to determine the status of individual status bits. The decimal-weighted value of the register is returned. The only bit used is bit 0 (LOSS), which indicates loss of the time reference due to a change in the reference clock signal. Reporting of event register bits in the status register system is controlled by the mask loaded into the enable register. All true event bits, that are enabled, are logically OR'ed, which results in setting true bit 11 (LOSS) of the Operation Status Register.

Precision Timebase Register Commands
Register Read Write Command
Event ♦   :STATus:PTIMebase:EVENt?
Enable (mask) ♦ ♦ :STATus:PTIMebase:ENABle
Precision Timebase Status Registers
Bit 7 6 5 4 3 2 1 0
Bit
Weight
128 64 32 16 8 4 2 1
Event
Register
— — — — — — — LOSS
Enable
Register
               
Sets to Bit 11 (PTIME) of Operation Status Register

Bit Definitions

LOSS
A true indicates that the precision timebase (provided by an 86107A or 86108A module) has detected a time reference loss due to a change in the amplitude or frequency of the reference clock signal.