:STATus:PTIMebase:ENABle

Instrument:
N1010A
N1000A
DCA-M
Meas. mode:
Scope
Eye
Jitter
TDR
Flex Apps:
FlexDCA
FlexRT

Command Syntax

:STATus:PTIMebase:ENABle <mask>

<mask> is an integer, 0 to 255, representing a mask for the bits in the event register.

Query Syntax

:STATus:PTIMebase:ENABle?

Description

Enters a decimal-weighted value in the precision timebase enable register that masks the ability to report bits in the precision timebase event register.

Precision Timebase Register Commands
Register Read Write Command
Event ♦   :STATus:PTIMebase:EVENt?
Enable (mask) ♦ ♦ :STATus:PTIMebase:ENABle
Precision Timebase Status Registers
Bit 7 6 5 4 3 2 1 0
Bit
Weight
128 64 32 16 8 4 2 1
Event
Register
— — — — — — — LOSS
Enable
Register
               
Sets to Bit 11 (PTIME) of Operation Status Register

Bit Definitions

LOSS
A true indicates that the precision timebase (provided by an 86107A or 86108A module) has detected a time reference loss due to a change in the reference clock signal.