:STATus:MTESt:EVENt?

Instrument:
N1010A
N1000A
DCA-M
Meas. mode:
Scope
Eye
Jitter
TDR
Flex Apps:
FlexDCA
FlexRT

Query Syntax

:STATus:MTESt:EVENt?

Description

Reads the mask test event register to determine the status of individual status bits. The decimal-weighted value of the register is returned. The only bit used is bit 0 (COMP), which indicates if an mask limit test has completed. Reporting of event register bits in the status register system is controlled by the mask loaded into the enable register. All true event bits, that are enabled, are logically OR'ed, which results in setting true bit 10 (MTEST) of the Operation Status Register. Use the :LTESt:MTESt:STATE command to configure a mask limit test.

Mask Test Register Commands
Register Read Write Command
Event ♦   :STATus:MTESt:EVENt?
Enable (mask) ♦ ♦ :STATus:MTESt:ENABle
Mask Test Status Registers
Bit 7 6 5 4 3 2 1 0
Bit
Weight
128 64 32 16 8 4 2 1
Event
Register
— — — — — — — COMP
Enable
Register
               
Sets to Bit 10 (MTEST) of Operation Status Register

Bit Definitions

COMP
A true indicates that the mask test has completed.