:STATus:OPERation:EVENt?

Instrument:
N1010A
N1000A
DCA-M
Meas. mode:
Scope
Eye
Jitter
TDR
Flex Apps:
FlexDCA
FlexRT
FlexPLL

Query Syntax

:STATus:OPERation:EVENt?

Description

Reads and clears the operation event register which contains bits that are set by various reporting registers. These reporting registers are identified in the Bit Definitions section of this topic.

Operation Register Commands
Register Read Write Command
Event ♦   :STATus:OPERation:EVENt?
Enable (mask) ♦ ♦ :STATus:OPERation:ENABle
Operation Status Registers for FlexDCA
Bit 15 14 13 12 11 10 9 8 7 6 5 4 3 2 1 0
Bit
Weight
32,768 16,384 8,192 4,096 2,048 1,024 512 256 128 64 32 16 8 4 2 1
Event
Register
— CAL — JIT PTIME MTEST ACQ LTEST CLCK RDCA — DAS LLINE — — —
Enable
Register
                               
Sets to Bit 7 (OPER) of Status Byte Register

Bit Definitions

ACQ
True indicates that an enabled bit in the acquisition event status register has been set and that the data acquisition has satisfied the specified completion criteria.
CAL
True indicates that an enabled bit in the calibration event status register has been set by a calibration completing.
CLCK
True indicates that an enabled bit in the clock recovery event status register has been set.
DAS
True indicates that an enabled bit in the repository event status register has been set.
JIT
True indicates that an enabled bit in the jitter event status register has been set. This occurs when there is a failure or an Auto Scale is needed.
LLINE
True indicates that an enabled bit in the limit line event status register has been set by a limit-line based limit test completing or failing.
LTEST
True indicates that an enabled bit in the limit test event status register has been set by a limit test completing or failing.
MTEST
True indicates that an enabled bit in the mask test event status register has been set by a mask test completing or failing.
PTIME
True indicates that an enabled bit in the precision timebase event status register has been set. This occurs when there is a loss of the precision timebase reference.
RDCA
True indicates that an enabled bit in the RDCA (Remote DCA) event status register has been set.