:CALibrate:OPTical:CONFirm

Flex Apps:
FlexOTO
FlexOTO Instance:
Hardware Diagram
Stations

Command Syntax

:CALibrate:OPTical:CONFirm

Description

During an ?

Requires FlexOTO revision A.07.60 and above.

Example Command Sequence

This example shows the steps used to update an optical path in an existing optical calibration. The updated calibration is then saved to a new file rather than just updating the existing file.

:CALibrate:OPTical:LOAD:FNAMe "%USER_DATA_DIR%\Optical Calibrations\OpticalCalibration_2024-02-12_1.ocdx"
:CALibrate:OPTical:LOAD
:CALibrate:OPTical:UPDate
:CALibrate:OPTical:SDONe?
:CALibrate:OPTical:STEP:SELect 3
:CALibrate:OPTical:SDONe?
:CALibrate:OPTical:OPOWer 4.50E-4
:CALibrate:OPTical:MATTenuation 1.00E+1
:CALibrate:OPTical:CONTinue
:CALibrate:OPTical:SDONe?
:CALibrate:OPTical:SPARtial
:CALibrate:OPTical:SDONe?
:CALibrate:OPTical:LOAD:FNAMe "%USER_DATA_DIR%\Optical Calibrations\OpticalCalibration_2024-updated.ocdx"
:CALibrate:OPTical:CONTinue
*OPC?