:CALibrate:OPTical:UPDate
Flex Apps:
FlexOTO
FlexOTO Instance:
Hardware Diagram
Command Syntax
:CALibrate:OPTical:UPDate <optical-input-power>
Query Syntax
:CALibrate:OPTical:UPDate?
Description
During the calibration for each optical path (lane), an optical source is used to inject a signal of known power into the lane being calibrated. Use this command to enter the average optical power measured for the input to current calibration of a Fixture Lane. Or, accept the current value. Use an optical power meter or DCA-X oscilloscope to measure the average optical power of the optical source. The average optical power must be between 100 μW and 5 mW.
Requires FlexOTO revision A.07.60 and above.