:CALibrate:OPTical:SPARtial
Command Syntax
:CALibrate:OPTical:SPARtial
Description
During an optical path calibration, send this command to save a partial calibration before all optical paths have been calibrated. This command is equivalent to clicking Save Current Calibration Data and Exit in the Optical Calibration dialog. If the calibration is new, use the :CALibrate:OPTical:LOAD:FNAMe command to enter a new name for the calibration, or use the :CALibrate:OPTical:CONTinue command to accept the automatically assigned name. A partial calibration can be opened, modified, completed, or used to perform Station measurements at any time.
Requires FlexOTO revision A.07.60 and above.
Example Command Sequence
This example shows the steps used to update an optical path in an existing optical calibration. The updated calibration is then saved to a new file rather than just updating the existing file.
:CALibrate:OPTical:LOAD:FNAMe "%USER_DATA_DIR%\Optical Calibrations\OpticalCalibration_2024-02-12_1.ocdx" :CALibrate:OPTical:LOAD :CALibrate:OPTical:UPDate :CALibrate:OPTical:SDONe? :CALibrate:OPTical:STEP:SELect 3 :CALibrate:OPTical:SDONe? :CALibrate:OPTical:OPOWer 4.50E-4 :CALibrate:OPTical:MATTenuation 1.00E+1 :CALibrate:OPTical:CONTinue :CALibrate:OPTical:SDONe? :CALibrate:OPTical:SPARtial :CALibrate:OPTical:SDONe? :CALibrate:OPTical:LOAD:FNAMe "%USER_DATA_DIR%\Optical Calibrations\OpticalCalibration_2024-updated.ocdx" :CALibrate:OPTical:CONTinue *OPC?