File | Instrument | Response | Stimulus | Utility | Cal | Apps | Remote ONLY
Get and Put Data: Measurement | Cal
| Power Cal | Custom
| Power Range
Other: GPIB
Pass-through | VISA
Pass-through | Capabilities
| Status/Events
| Rear-panel
| FIFO
and FastCW | Speed
up Measurements! | Ground Loop
Description |
SCPI |
COM |
---|---|---|
Get X-Axis values (variant) |
||
Get X-Axis values (typed) |
None |
|
Set/get X-axis for trace |
None |
|
Set/get the X-Axis domain |
None |
|
Get X-Axis values (Meas object) |
None |
|
Get typed complex data from the specified location. Returned in two arrays. |
None |
|
Get typed NAComplex data from the specified location. Returned in one array. |
None |
|
Get typed data pairs from the specified location. Returned in two arrays. |
None |
|
Get typed scalar data from the specified location. Returned in one array. |
None |
|
Get variant data from the specified location in a SPECIFIED FORMAT. Returned in one array. |
None |
|
Get receiver data |
All of the above |
|
Specifies ASCII or REAL type for data transfers |
None |
|
Get complex or formatted data from the measurement or memory result buffer |
All of the above |
|
Get the formatted data array of multiple traces of the selected channel. |
None |
|
Get the corrected data array of multiple traces of the selected channel. |
None |
|
Gets SnP data for the specified ports. |
||
Get ALL SnP data |
||
Put Measurement Data INTO the Analyzer |
||
Put complex data into the specified location. |
None |
|
Put typed NAComplex data into the specified location. |
None |
|
Put scalar data into the measurement result location. |
None |
|
Put complex Variant data into the specified location. |
None |
|
Put complex or formatted data into the measurement or memory result buffer |
None |
|
Get complex Error Term data |
None |
|
Get variant Error Term data |
||
Get variant Error Term data by text filter |
||
Get complex Standard data |
None |
|
Get variant Standard data |
None |
|
Get variant Standard data by text filter |
None |
|
Put complex Error Term data |
None |
|
Put variant Error Term data |
||
Put complex Standard data |
None |
|
Put variant Standard data |
None |
|
Get variant cal data |
||
Get typed cal data |
||
Put variant cal data |
||
Put typed cal data |
||
Get and Put Custom data |
Many queries regarding the capability of a specific PNA |
||
PXIe module queries |
|
|
Read installed options |
Set/get list of discrete frequencies corresponding to powers |
||
Get a single max leveled power value |
||
Get an array of max leveled power values |
||
Get a single minimum leveled power value |
||
Get an array of minimum leveled power values |
||
Set/get name of the value for the given path element name |
SYSTem:CAPability:HARDware:POWer:PATH:CONFig:ELEMent[:STATe] |
|
Get all RF path element names |
SYSTem:CAPability:HARDware:POWer:PATH:CONFig:ELEMent:CATalog? |
|
Set/get port number for power data |
||
Set/get type of power range data to be returned |
||
Get minimum of all max leveled power values |
||
Get maximum of all minimum power values |
||
Set/get lower bound of the frequency range |
||
Set/get upper bound of the frequency range |
||
Reset all Power Range properties to default values |
Status Registers |
None |
|
*OPC;*WAI |
None |
AllowAllEvents Method |
None |
|
AllowEventCategory Method |
None |
|
AllowEventMessage Method |
None |
|
AllowEventSeverity Method |
None |
|
DisallowAllEvents Method |
None |
|
MessageText Method |
None |
|
OnCalEvent |
None |
|
OnChannelEvent |
None |
|
OnDisplayEvent |
None |
|
OnHardwareEvent |
None |
|
OnMeasurementEvent |
None |
|
OnSCPIEvent |
None |
|
OnSystemEvent |
None |
|
OnUserEvent |
None |
|
SetFailOnOverRange |
None |
Material Handler I/O Connector |
||
Auxiliary IO Connector |
||
External Test Set Connector |
FIFO ON|OFF |
||
Read number of data points |
||
Read data |
||
Read data compact form |
None |
|
Clear data |
||
Returns a specific number of bytes to read |
||
Reads the FIFO buffer data as a Variant of a specified array size (SafeArray) of bytes. |
||
Reads the FIFO buffer data as a Variant of a specified array size (SafeArray) of 32-bit floating point (Float32) numbers. |
|
|
Reads the FIFO buffer data as a Variant of a specified array size (SafeArray) of 16-bit integers. |
|
|
Reads the FIFO buffer data as a Variant of a specified array size (SafeArray) of 32-bit integers. |
|
Other N5264A Commands |
||
FastCW |
||
Enable Point Averaging |
||
Enable Point Sweep |
||
Set Trace Sweep |
De-embedding |
|
Sets and returns the Capacitance value |
|
Sets and returns the Inductance value |
|
Sets and returns the Resistance value |
|
Turns ON or OFF De-embedding |
|
Specifies the circuit model type |
|
Specifies the filename of the s1p file to load |
|
Embedding |
|
Sets and returns the Capacitance value |
|
Sets and returns the Inductance value |
|
Sets and returns the Resistance value |
|
Turns ON or OFF Embedding |
|
Specifies the circuit model type |
|
Specifies the filename of the s1p file to load |