File  |  Instrument  |  Response  |  Stimulus  |  Utility  |  Cal  |  Apps  |  Remote ONLY


Frequency | Offset | Power | ALC | Recvr Lvl | Source Ports| # Points | Trigger :Ext | Auxiliary Trigger
Sweep settings:..Time | Setup | Segment | Power | Phase | Pulse Setup | DC Sources | Multi-Dimensional Sweep | Global Source

See Remotely Specifying a Source Port .

Description

SCPI

COM

Frequency

Start Freq

SENSe:FREQuency:STARt

chan.StartFrequency

Stop Freq

SENSe:FREQuency:STOP

chan.StopFrequency

Center Freq

SENSe:FREQuency:CENTer

chan.CenterFrequency

Span

SENSe:FREQuency:SPAN

chan.FrequencySpan

CW Frequency

SENSe:FREQuency:CW

chan.CWFrequency

Number of Points

SENSe:SWEep:POINts

chan.NumberOfPoints

Step size

SENSe:SWEep:STEP

FrequencyStep Property

Frequency Offset Commands

Freq Offset ON/Off

SENSe:FOM[:STATe]

FOM.State

Read available ranges

SENSe:FOM:CATalog?

Read number of ranges

SENSe:FOM:COUNt?

RangeCount

X-Axis display range

SENSe:FOM:DISPlay:SELect

DisplayRange

Read range name

SENSe:FOM:RANGe:NAME?

Name FOMRange

Read range number

SENSe:FOM:RNUM?

rangeNumber

Set range coupling

SENSe:FOM:RANGe:COUPled

Coupled

Set sweep type

SENSe:FOM:RANGe:SWEep:TYPE

SweepType

Set CW freq

SENSe:FOM:RANGe:FREQuency:CW

CWFrequency

Set start freq

SENSe:FOM:RANGe:FREQuency:STARt

StartFrequency

Set stop freq

SENSe:FOM:RANGe:FREQuency:STOP

StopFrequency

Set offset value

SENSe:FOM:RANGe:FREQuency:OFFSet

Offset

Set divisor value

SENSe:FOM:RANGe:FREQuency:DIVisor

Divisor

Set multiplier value

SENSe:FOM:RANGe:FREQuency:MULTiplier

Multiplier

Freq. Offset Segment Sweep

ON|OFF

SENSe:FOM:RANGe:SEGMent

State

Add a segment

SENSe:FOM:RANGe:SEGMent:ADD

FOM.Add

Delete a segment

SENSe:FOM:RANGe:SEGMent:DELete

Remove

Count the segments

SENSe:FOM:RANGe:SEGMent: COUNT?

Count

Center Frequency

SENSe:FOM:RANGe:SEGMent:FREQuency:CENTer

CenterFrequency

Frequency Span

SENSe:FOM:RANGe:SEGMent:FREQuency:SPAN

FrequencySpan

Start Frequency

SENSe:FOM:RANGe:SEGMent:FREQuency:STARt

StartFrequency

Stop Frequency

SENSe:FOM:RANGe:SEGMent:FREQuency:STOP

Stop Frequency

Number of Points

SENSe:FOM:RANGe:SEGMent:SWEep:POINts

Number of Points

IF Bandwidth value

SENSe:FOM:RANGe:SEGMent:BWID

IF Bandwidth

IF Bandwidth control

SENSe:FOM:RANGe:SEGMent:BWID:CONTrol

IF BandwidthOption

Source Power value

SENSe:FOM:RANGe:SEGMent:POWer

Test Port Power

Source Power control

SENSe:FOM:RANGe:SEGMent:POWer:CONTrol

Source Power Option

Sweep time value

SENSe:FOM:RANGe:SEGMent:SWEep:TIME

Sweep Time

Sweep time control

SENSe:FOM:RANGe:SEGMent:SWEep:TIME:CONTrol

TimeOption

Test Set Switch

ROUT:PATH:LOOP:R1

chan.R1InputPath

Power Settings    See Remotely Specifying a Source Port .

Power ON | OFF

OUTP

app.SourcePowerState

Source Power (Auto | ON | OFF)

SOURce:POWer:MODE

SourcePortMode

Power Value

SOURce:POWer[:LEVel][:IMMediate][:AMPLitude]

chan.TestPortPower

Port Selection

SENSe:SWepE:SRCPort

chan.TestPortPower

Couple Ports OFF | ON

SOURce:POWer:COUPle

chan.CouplePorts

Attenuator Mode Auto|Manual

SOURce:POWer:ATTenuation:Auto

chan.AttenuatorMode

Attenuation Value

SOURce:POWer:ATTenuation

chan.Attenuator

Power Slope ON | OFF

SOURce:POWer:SLOPe:STATe

chan.PowerSlopeState

Power Slope Value

SOURce:POWer:SLOPe

chan.PowerSlope

Receiver Attenuation

SENSe:POWer:ATTenuator

chan.ReceiverAttenuator

Receiver Reference Attenuation

SOURce:POWer:ATTenuation:RECeiver:REFerence

None

Receiver Test Attenuation

SOURce:POWer:ATTenuation:RECeiver:TEST

None

Shutdown or Restart System

SYSTem:POFF

None

See also Power Range remote commands

Power Limit and Offsets

Set power limit

SYSTem:POWer:LIMit

Limit

Set Calibration power limit

SYSTem:POWer:LIMit:CALibration

None

Power limit ON/OFF

SYSTem:POWer:LIMit:STATe

State

Power limit UI lock

SYSTem:POWer:LIMit:LOCK

Lock

Set offset value

SOURce:POWer:ALC:MODE:RECeiver:OFFSet

PowerOffset

Receiver Leveling

Rx Level ON|OFF

SOURce:POWer:ALC:MODE:RECeiver

State

Select the reference receiver

SOURce:POWer:ALC:MODE:RECeiver:REFerence

ReferenceReceiver

Sets all ports to pre-sweep or point leveling mode for the specified channel.

SOURce:POWer:ALC[:MODE]:RECeiver:ACQuisition:MODE

None

Enables or disables the receiver leveling maximum iteration search function.

SOURce:POWer:ALC[:MODE]:RECeiver:ITERation:ENABle

None

Set maximum iterations

SOURce:POWer:ALC:MODE:RECeiver:ITERation:VALue

IterationNumber

Set tolerance

SOURce:POWer:ALC:MODE:RECeiver:TOLerance

Tolerance

Set offset value

SOURce:POWer:ALC:MODE:RECeiver:OFFSet

PowerOffset

Separate IFBW

SOURce:POWer:ALC:MODE:RECeiver:FAST

FastMode

Set Rx IFBW

SOURce:POWer:ALC:MODE:RECeiver:IFBW

LevelingIFBW

Safe mode ON|OFF

SOURce:POWer:ALC:MODE:RECeiver:SAFE

SafeMode

Safe mode Max power

SOURce:POWer:ALC:MODE:RECeiver:SAFE:MAX

PowerMax

Safe mode Min power

SOURce:POWer:ALC:MODE:RECeiver:SAFE:MIN

PowerMin

Use Last Result for Source Power Cal

SOURce:POWer:ALC:MODE:RECeiver:LSPC

LastLevelingAsSPC

Sets the specific PULSe4 behavior.

SENSe:PULSe4:MODE

None

Sets all ports to pre-sweep or point leveling mode for the specified channel.

SOURce:POWer:ALC[:MODE]:RECeiver:ACQuisition:MODE

None

Enables or disables the receiver leveling maximum iteration search function.

SOURce:POWer:ALC[:MODE]:RECeiver:ITERation:ENABle

None

ALC Leveling

Returns list of valid ALC Leveling Modes

SOURce:POWer:ALC:MODE:CATalog?

GetSupportedALCModes

Set ALC Mode

SOURce:POWer:ALC[:MODE]

ALCLevelingMode

Specifying Source Ports  See Remotely Specifying a Source Port.

Returns the number of source ports.

None

SourcePortCount

Returns the string names of source ports.

SOURce:CATalog?

SourcePortNames

Returns the source port number of the specified string port name.

None

GetPortNumber

IF Bandwidth

IF Bandwidth

SENSe:BANDwidth | BWIDth[:RESolution]

chan.IFBandwidth

Previous IF Bandwidth

None

chan.Previous_IFBandwidth

Next IFBandwidth

None

chan.Next_IFBandwidth

Reduce IF BW

SENSe:BANDwidth | BWIDth:TRACk

chan.ReduceIFBW

Sweep

Sweep Time Value

SENSe:SWEep:TIME:AUTO

chan.SweepTime

Returns the time the first point of a Time Sweep is measured.

SENSe:SWEep:TIME:STARt?

None

Sets the time the analyzer takes to complete one sweep.

SENSe:SWEep:TIME[:STOP]

None

Sweep Setup

Number of Points

SENSe:SWEep:POINts

chan.NumberOfPoints

Sweep Type (Lin | Pwr | CW | Seg | Phase)

SENSe:SWEep:TYPE

chan.SweepType

Sweep Generation (Stepped | Analog)

SENSe:SWEep:GENeration

chan.SweepGenerationMode

Dwell Time Value

SENSe:SWEep:DWEL

chan.DwellTime

Dwell Time Auto  set the minimum dwell time

SENSe:SWEep:DWEL:AUTO

chan.DwellTime

Sweep Delay

SENSe:SWEep:DWELl:SDELay

SweepDelay

Alternate Sweeps

SENSe:COUPle

chan.AlternateSweep

External ALC

SOURce:POWer:DETector

app.ExternalALC

Enable Point Sweep

SENSe:SWEep:GENeration:POINtsweep

PointSweepState

Fast Sweep

SENSe:SWEep:SPEed

SweepSpeedMode

Fast CW

SENSe:SWEep:TYPE:FACW

FastCWPointCount

Set shift LO maximum frequency

SENSe:SWEep:SLOCal:MAXimum

None

Turn shift LO on or off

SENSe:SWEep:SLOCal:STATe

None

Returns whether or not the VNA has the low frequency extension (LFE) installed.

SYSTem:CAPability:HARDware:LFEXtension:EXISts?

HasLowFrequencyExtension

Turns ON or OFF low frequency extension

SENSe:SWEep:LFEXtension:STATe

LowFrequencyExtension

Power Sweep

Start Power

SOURce:POWer:STARt

chan.StartPower

Stop Power

SOURce:POWer:STOP

chan.StopPower

Center

SOURce:POWer:CENTer

Span

SOURce:POWer:SPAN

Segment Sweep

ON|OFF

SENSe:SEGMent[:STATe]

Seg.State

Add a segment

SENSe:SEGMent:ADD

Segs.Add

Delete a segment

SENSe:SEGMent:DELete

segments.Remove

Delete all segments

SENSe:SEGMent:DELete:ALL

None

Count the segments

SENSe:SEGMent:COUNt

chans.Count

Read the segment number

None

seg.SegmentNumber

Segment Center Frequency

SENSe:SEGMent:FREQuency:CENTer

chan.centerFrequency

Segment Frequency Span

SENSe:SEGMent:FREQuency:SPAN

chan.FrequencySpan

Segment Start Frequency

SENSe:SEGMent:FREQuency:STARt

Chan.StartFrequency

Segment Stop Frequency

SENSe:SEGMent:FREQuency:STOP

Chan.StopFrequency

Number of Points

SENSe:SEGMent:SWEep:POINt

seg.NumberOfPoints

IF Bandwidth

SENSe:SEGMent:BWIDth

seg.IFBandwidth

IF Bandwidth Option

SENSe:SEGMent:BWIDth:CONTrol

segs.IFBandwidthOption

IF Bandwidth Per Port

SENSe:SEGMent:BWIDth:PORT:CONTrol

PortIFBandwidthOption

PortIFBandwidth

Sweep Delay Time

SENSe:SEGMent:SWEep:DELay

DelayOption

Delay

Sweep Dwell

SENSe:SEGMent:SWEep:DWELl

SweepTimeOption

DwellTime

Sweep Mode

SENSe:SEGMent:SWEep:GENeration

SweepModeOption

SweepMode

Total Sweep Points

SENSe:SEGMent:SWEep:POINts:TOTal?

NumberOfPoints

Total Sweep Time

SENSe:SEGMent:SWEep:TIME:TOTal?

None

Source Power

SENSe:SEGMent:POWer

chan.TestPortPower

Source Power Option

SENSe:SEGMent:POWer:CONTrol

segs.SourcePowerOption

X-Axis Point Spacing

SENSe:SEGMent:X:SPACing

chan.XAxisPointSpacing

Allow Arbitrary Segments

SENSe:SEGMent:ARBitrary

segs.AllowArbitrarySegments

Upload a segment table

SENSe:SEGMent:LIST

SetAllSegmernts

Download a segment table

SENSe:SEGMent:LIST

GetAllSegments

Sweep delay ON|OFF

SENSe:SEGMent:SWEep:DELay:CONTrol

DelayOption

Sweep dwell ON|OFF

SENSe:SEGMent:SWEep:DWELl:CONTrol

SweepTimeOption

IF Bandwidth resolution

SENSe:SEGMent:BWIDth:PORT[:RESolution]

PortIFBandwidthOption

PortIFBandwidth

Sets or returns the SA data threshold

SENSe:SEGMent:SA:DTHReshold

SADataThreshold

Specifies whether SA Data Threshold can be set independently for each segment

SENSe:SEGMent:SA:DTHReshold:CONTrol

SADataThresholdOption

Sets or returns the SA multitone reference

SENSe:SEGMent:SA:MTReference

SAMTReference

Specifies whether SA Reference Tone can be set independently for each segment

SENSe:SEGMent:SA:MTReference:CONTrol

SAMTReferenceFreqOption

Queries the maximum value of the SA Reference Tone

SENSe:SEGMent:SA:MTReference:MAX?

None

Queries the minimum value of the SA Reference Tone

SENSe:SEGMent:SA:MTReference:MIN?

None

Sets or returns the SA vector average

SENSe:SEGMent:SA:VAVerage

SAVectorAverage

Specifies whether SA Vector Averaging can be set independently for each segment

SENSe:SEGMent:SA:VAVerage:CONTrol

SAVectorAverageOption

Sets or returns the SA video bandwidth

SENSe:SEGMent:SA:VIDeobw

SAVideoBandwidth

Sets or returns the noise figure bandwidth.

SENSe:SEGMent:NFBW

NoiseFigureBW

Turns ON or OFF the noise figure bandwidth setting.

SENSe:SEGMent:NFBW:CONTrol

NoiseFigureBWOption

Specifies whether SA Video Bandwidth can be set independently for each segment

SENSe:SEGMent:SA:VIDeobw:CONTrol

SAVideoAverageOption

Source Phase Control / Sweep

Phase Sweep type

SENSe:SWEep:TYPE

SweepType

Set fixed phase value

SOURce:PHASe [:FIXed]

FixedPhase

Phase sweep start value

SOURce:PHASe:STARt

StartPhase

Phase sweep stop value

SOURce:PHASe:STOP

StopPhase

Phase parameter

SOURce:PHASe:PARameter

PhaseParameter

Set Phase control mode

SOURce:PHASe:PARameter:MODE

PhaseControlMode

Set reference port

SOURce:PHASe:PARameter:PORT

PhaseReferencePort

Read available phase control modes for the port

SOURce:PHASe:PARameter:MODE:CAT?

PhaseParameterModes

Couple sweep settings

SOURce:PHASe:CONTrol:COUPle

CouplePhasePortSettings

Set number of sweep iterations

SOURce:PHASe:CONTrol:ITERation

PhaseIterationNumber

Set sweep tolerance

SOURce:PHASe:CONTrol:TOLerance

PhaseTolerance

Set and read an array of phase offsets.

SOURce:PHASe:CORRection:DATA

PhaseCorrectionData

Use phase offset array.

SOURce:PHASe:CORRection:STATe

PhaseCorrectionEnabled

Set and read an array of ratioed power offsets.

SOURce:PHASe:POFFset:CORRection:DATA

RatioedPowerCorrectionData

Use power offset array.

SOURce:PHASe:POFFset:CORRection:STATe

RatioedPowerCorrectionEnabled

Set the fixed power ratioed value

SOURce:PHASe:POFFset:FIXed

FixedRatioedPower

Set the start power ratioed value.

SOURce:PHASe:POFFset:STARt

StartRatioedPower

Set the stop power ratioed value.

SOURce:PHASe:POFFset:STOP

StopRatioedPower

Returns the available internal ports that the external port can be set to.

SOURce:PHASe:EXTernal:CATalog?

None

Sets and returns the internal port that the external port is routed through.

SOURce:PHASe:EXTernal:PORT

None

Returns the available phase control modes for the specified port.

SOURce:PHASe:MODE:CATalog?

None

Sets and returns the Phase Control mode.

SOURce:PHASe:MODE[:VALue]

None

Returns the available parameters.

SOURce:PHASe:PARameter[:CATalog?

None

Sets and returns the ratioed receivers (parameter) to use for phase control.

SOURce:PHASe:PARameter[:VALue]

None

Returns the available ports that can be used as phase control reference ports for the phase controlled port.

SOURce:PHASe:REFerence:CATalog?

None

Sets and returns the reference port for the Phase Control measurement.

SOURce:PHASe:REFerence:PORT

None

Trigger

Source (where trigger comes from)

Source (Int | Ext | Manual)

TRIGger[:SEQuence]:SOURce

trigSetup.Source

Internal | Manual

INITiate:CONTinuous

None

Trigger! (for Manual Source)

INITiate[:IMMediate]

app.ManualTrigger

Scope (what is triggered)

Scope (Global | Channel)

TRIGger[:SEQuence]:SCOPe

trigSetup.Scope

Channel Settings (how the channel responds to triggers)

Continuous

SENSe:SWEep:MODE CONTinous

chan.Continuous

Read Continuous Mode

None

chan.IsContinuous

Number of Groups

SENSe:SWEep:GROup:COUNt

chan.NumberOfGroups

Read Groups

None

chan.GetNumberOfGroups

Hold

SENSe:SWEep:MODE HOLD

chan.Hold

Hold Mode (read-only)

None

chan.IsHold

All channels in Hold

SYSTem:CHANnels:HOLD

chans.Hold

All channels Resume

SYSTem:CHANnels:RESume

chans.Resume

Single

SENSe:SWEep:MODE SINGle

chan.Single

Trigger Mode

SENSe:SWEep:TRIGger:MODE

chan.TriggerMode

Restart

INITiate[:IMMediate]

None

Abort

ABORt

chan.Abort

External Meas Trigger Input

Scope (Global/Chan)

TRIGger[:SEQuence]:SCOPe

trigSetup.Scope

Trigger Delay (Global)

TRIGger:DELay

app.TriggerDelay

Trigger Delay (Channel)

SENSe:SWEep:TRIGger:DELay

chan.ExternalTriggerDelay

MeasTrigIn/ Hand I/O

TRIGger:ROUTE:INPut

ExternalTriggerConnectionBehavior

Level or Edge

TRIGger:TYPE

ExternalTriggerConnectionBehavior

Neg/Low or Pos/High

TRIGger:SLOPE

ExternalTriggerConnectionBehavior

Accept Trigger Before Armed

CONTrol:SIGNal:TRIGger:ATBA

AcceptTriggerBeforeArmed

Ready for Trigger Indicator (Out)

MeasTrig Rdy/ Hand I/O

TRIGger:ROUTE:READy

CONTrol:SIGNal:STReamline:RTRigger[:STATe]

CONTrol:SIGNal:PXI:RTRigger[:STATe]

CONTrol:SIGNal:STReamline:RTRigger:ROUTe

CONTrol:SIGNal:PXI:RTRigger:ROUTe

None

Checks if the PNA is ready for a hardware trigger

TRIGger:STATus:READy?

ReadyForTriggerStatus

High / Low

TRIGger:READy:POLarity

ReadyForTriggerPolarity

Auxiliary Triggering (PNA-X and N522x models)

Which AuxTrig connector pair being used.

N/A

Number

How many Aux connector pairs.

TRIGger:AUXiliary:COUNt?

AuxiliaryTriggerCount

AUX TRIG OUT

Enable

TRIGger:CHANnel:AUXiliary

Enable

Global or Channel Pref.

TRIGger:PREFerence:AIGLobal

AuxTriggerScopeIsGlobal

Polarity (Pos/Neg)

TRIGger:CHANnel:AUXiliary:OPOLarity

TriggerOutPolarity

Position (Before/After acq)

TRIGger:CHANnel:AUXiliary:POSition

TriggerOutPosition

OUT Pulse width

TRIGger:CHANnel:AUXiliary:DURation

TriggerOutDuration

Point or Sweep.

TRIGger:CHANnel:AUXiliary:INTerval

TriggerOutInterval

Rear SMB

CONTrol:SIGNal:STReamline:TRIGger:OUTPut[:STATe]

CONTrol:SIGNal:STReamline:TRIGger:OUTPut:ROUTe

Backplane

CONTrol:SIGNal:PXI:TRIGger:OUTPut[:STATe]

CONTrol:SIGNal:PXI:TRIGger:OUTPut:ROUTe

AUX TRIG (Ready) IN

Enable Handshake

TRIGger:CHANnel:AUXiliary:HANDshake

HandshakeEnable

Edge or Level

Level NOT in UI.

TRIGger:CHANnel:AUXiliary:TYPE

TriggerInType

Polarity High/leading or Low/trailing.

TRIGger:CHANnel:AUXiliary:IPOLarity

TriggerInPolarity

Delay

TRIGger:CHANnel:AUXiliary:DELay

Delay

Pulse Measurement Setup (PNA-X)

Pulse Meas Mode

SENSe:SWEep:PULSe:MODE

PulseMeasMode

Autodetect Pulse mode

SENSe:SWEep:PULSe:DETectmode

AutoDetection

Set Pulse Mode (Narrow | Wide)

SENSe:SWEep:PULSe:WIDeband

WideBandDectionState

Autoselect IFBW

SENS:SWEep:PULSe:CWTime[:AUTO]

AutoIFBandWidth

Autoselect IF Gain

SENSe:SWEep:PULSe:IFGain

None

Autoselect Pulse clock period

SENSe:SWEep:PULSe:PRF

AutoOptimizePRF

Autoselect Width and Delay

SENSe:SWEep:PULSe:TIMing

AutoPulseTiming

Autoselect Pulse Gens

SENSe:SWEep:PULSe:DRIVe

AutoSelectPulseGen

Autoselect CW Sweep Time

SENSe:SWEep:PULSe:CWTime

AutoCWSweepTime

Pulse (manual) Settings

Set master pulse frequency

SENSe:SWEep:PULSe:MASTer:FREQuency

MasterFrequency

Set master pulse period

SENSe:SWEep:PULSe:MASTer:PERiod

MasterPeriod

Set master pulse width

SENSe:SWEep:PULSe:MASTer:WIDTh

MasterWidth

Set pulse start time

SENSe:SWEep:PULSe:PROFile:STARt

PulseProfileStart

Set pulse stop time

SENSe:SWEep:PULSe:PROFile:STOP

PulseProfileStop

Pulse Generators (PNA-X)

Enable Pulse output ON | OFF

SENSe:PULSe<n>[:STATe]

State

Set Pulse Period for ALL pulse generators

SENSe:PULSe:PERiod

Period

Set Pulse Delay

SENSe:PULSe<n>:DELay

Delay

Set Pulse Width

SENSe:PULSe<n>:WIDTh

Width

Set Pulse delay increment

SENSe:PULSe<n>:DINCrement

DelayIncrement

Enables Subpoint triggering

SENSe:PULSe<n>:SUBPointtrig

SubPointTrigger

Set Pulse Invert

SENSe:PULSe<n>:INVert

Invert

Internal Pulse Modulator Enable

Choose from element value 8 or 9

SENSe:PATH:CONFig:ELEMent

Element

Value

Returns the ADC delay.

SENSe:PULSe:HDELay:ADC?

ADCDelay

Sets the time lag between the pulse drive signal and the actual RF output.

SENSe:PULSe:HDELay:MODulator

ModulatorDelay

Enables / Disables offset delays.

SENSe:PULSe:HDELay[:STATe]

EnableOffsetDelays

Sets and reads the device being controlled by the pulse generator output.

SENSe:PULSe:MTIMing:DEVice

PulseTimingDevice

Enable pulse4 to monitor ADC activity.

SENSe:PULSe4:OPTion

Pulse4OutAsADCActivity

Sets the specific PULSe4 behavior.

SENSe:PULSe4:MODE

None

External Pulse Trigger (PNA-X)

PulseSyncIn Trigger Polarity

SENSe:PULSe:TPOLarity

TriggerInPolarity

PulseSyncIn Trigger Type

SENSe:PULSe:TTYPe

TriggerInType

Sync receiver to Pulse0

(enable pulse0)

SENSe:PULSe[:STATe]

pulse.State

Pulse Trigger Source

Choose element and setting

SENSe:PATH:CONFig:ELEMent

Element

Value

IF Path Configuration

DC Source Control

See Ext DC Device commands

Source names catalog

SOURce:DC:CATalog?

Sources

Enable source outputs

SOURce:DC:ENABle

EnableAllOutput

Source state

SOURce:DC:STATe

State

Start DC

SOURce:DC:STARt

Start

Stop DC

SOURce:DC:STOP

Stop

Data

SOURce:DC:DATA

ListData

Set and return the Max DC limit value for a DC source

SOURce:DC:LIMit:MAXimum

LimitMax

Set and return the Min DC limit value for a DC source

SOURce:DC:LIMit:MINimum

LimitMin

Multi-Dimensional Sweep

Set and read the order for the specified DC source in the multi-dimensional sweep.

SOURce:DC:DIMension:ORDer

DCOrder

Set and read the specified DC source’s ON/OFF state in the multi-dimensional sweep.

SOURce:DC:DIMension[:STATe]

DCState

Read the names of source domains in the multi-dimensional sweep whose state is ON and whose dimension order is the specified dimension order.

SOURce:DIMension:CATalog?

DimensionCatalog

Read the highest dimension order in the multi-dimensional sweep.

SOURce:DIMension:COUNt?

DimensionCount

Set and read the point count for the specified dimension order in the multi-dimensional sweep.

SOURce:DIMension:POINts

DimensionPointCount

Set and read the repeat count for the specified dimension order in the multi-dimensional sweep.

SOURce:DIMension:REPeat:COUNt

DimensionRepeatCount

Set and read the source frequency domain’s order in the multi-dimensional sweep.

SOURce:FREQuency:DIMension:ORDer

SourcePortFrequencyOrder

Set and read the source frequency domain’s ON/OFF state in the multi-dimensional sweep.

SOURce:FREQuency:DIMension[:STATe]

SourcePortFrequencyState

Set and read the fixed frequency value for a specific port.

SOURce:FREQuency:FIXed

SourcePortFixedFrequency

Set and read the start frequency value for a specific port.

SOURce:FREQuency:STARt

SourcePortStartFrequency

Set and read the stop frequency value for a specific port.

SOURce:FREQuency:STOP

SourcePortStopFrequency

Set and read the source phase domain’s order in the multi-dimensional sweep.

SOURce:PHASe:DIMension:ORDer

SourcePortPhaseOrder

Set and read the source phase domain’s ON/OFF state in the multi-dimensional sweep.

SOURce:PHASe:DIMension[:STATe]

SourcePortPhaseState

Set and read the source power domain’s order in the multi-dimensional sweep.

SOURce:POWer:DIMension:ORDer

SourcePortPowerOrder

Set and read the source power domain’s ON/OFF state in the multi-dimensional sweep.

SOURce:POWer:DIMension[:STATe]

SourcePortPowerState

Global Source Commands

Set and return the frequency of the specified global source.

SYSTem:PREFerences:SOURce:GLOBal:FREQuency

None

Set and return the output state of the specified global source.

SYSTem:PREFerences:SOURce:GLOBal:OUTPut[:STATe]

None

Set and return the global sources that ignore the power off setting.

SYSTem:PREFerences:SOURce:GLOBal:POFF:IGNore[:STATe]

None

Set and return the power of the specified global source.

SYSTem:PREFerences:SOURce:GLOBal:POWer

None

Set and return the global state of the specified global source.

SYSTem:PREFerences:SOURce:GLOBal[:STATe]

None

Loads the internal source modulation file.

SYSTem:PREFerences:SOURce:GLOBal:MODulation:LOAD

None

Returns the name of the currently loaded internal source modulation file.

SYSTem:PREFerences:SOURce:GLOBal:MODulation:FILE?

None

Set and return the state of the specified internal source modulation port.

SYSTem:PREFerences:SOURce:GLOBal:MODulation[:STATe]

None