:DISK:DWIZard:DHERtz{1:4}:SDATa
Command Syntax
:DISK:DWIZard:DHERtz{1:4}:SDATa {ON | OFF}
Description
When saving a Documentation Wizard zip file (:DISK:DWIZard:SAVE), use this command to add a ASCII data file (XY-value waveform file) for each displayed waveform in any Degrees (Hz) waveform content windows. Degrees (Hz) waveform content windows display waveforms from different sources:
- FFT function. Saves one waveform file for each displayed waveform (example, FFT[1] (F1).txt)
- S-parameter. Saves one waveform file for each displayed waveform (for example, S11 Phase.txt).
A screen capture each displayed Degrees (Hz) waveform content window is also saved (Degrees (Hz) N Window Screen Capture.png).
ON- Includes files in Documentation Wizard zip file.
OFF- Excludes files in Documentation Wizard zip file.
Query Syntax
:DISK:DWIZard:DHERtz:SDATa?
Query Response
{1 | 0}