:DISK:DWIZard:SSParam
Command Syntax
:DISK:DWIZard:SSParam {ON | OFF}
Description
When saving a Documentation Wizard zip file (:DISK:DWIZard:SAVE), use this command to add Touchstone S-parameter files.
Touchstone files can be imported into Keysight's Physical Layer Test Systems (PLTS) for further analysis. S-parameters cannot be imported back. However, S-parameters can be imported into the following Infiniium function operators:
- Apply s2p (
:FUNCtion:PARameters:CONVolve:FNAMe) - Apply s4p (
:FUNCtion:PARameters:DCONvolve:FNAMe) - Remove s2p (
:FUNCtion:PARameters:DEConvolve:FNAMe) - Remove s4p (
:FUNCtion:PARameters:DDEConvolve:FNAMe)
These operators are used to transform measured waveforms to compensate for the effects of various test-setup devices.
ON- Includes files in Documentation Wizard zip file.
OFF- Excludes files in Documentation Wizard zip file.
Query Syntax
:DISK:DWIZard:SSParam?
Query Response
{1 | 0}