:DISK:DWIZard:TIME{1:4}:SDATa
Command Syntax
:DISK:DWIZard:TIME{1:4}:SDATa {ON | OFF}
Description
When saving a Documentation Wizard zip file (:DISK:DWIZard:SAVE), use this command to add the following waveform data files associated with the Waveform content window:
- Waveform: ASCII XY-value waveform files (example, Channel 1_1 (1_1).txt)
- Eye diagram: color-grade gray-scale database waveform files (example, Channel 1_1 (1_1).cgsi)
A screen capture of the waveform content window is also saved (Waveform Window Screen Capture.png). The Waveform content window is the default window for viewing most waveforms.
ON- Includes files in Documentation Wizard zip file.
OFF- Excludes files in Documentation Wizard zip file.
Query Syntax
:DISK:DWIZard:TIME{1:4}:SDATa?
Query Response
{1 | 0}