:DISK:DWIZard:ECResults:SDATa
Command Syntax
:DISK:DWIZard:ECResults:SDATa {ON | OFF}
Description
When saving a Documentation Wizard zip file (:DISK:DWIZard:SAVE), use this command to add the results shown in the Eye Contours results table. The data is placed in a comma-delimited ASCII file (Eye Contours Window Results.csv). A screen capture of the Amplitude results table (Eye Contours Window Screen Capture.png) is also saved. The instrument must have the Eye Contours results table displayed.
ON- Includes files in Documentation Wizard zip file.
OFF- Excludes files in Documentation Wizard zip file.
Query Syntax
:DISK:DWIZard:ECResults:SDATa?
Query Response
{1 | 0}