:DISK:DWIZard:SSCReen

Command Syntax

:DISK:DWIZard:SSCReen {ON | OFF}

Description

When saving a Documentation Wizard zip file (:DISK:DWIZard:SAVE), use this command to add a screen capture of the entire Infiniium 2026 display (Entire UI Screen Capture.png).

If a displayed dialog box is outside Infiniium's window, it will not be included in the screen image capture. Use the Windows Print Screen function instead.

ON
Includes files in Documentation Wizard zip file.
OFF
Excludes files in Documentation Wizard zip file.

Query Syntax

:DISK:DWIZard:SSCReen?

Query Response

{1 | 0}