:DISK:DWIZard:LFMagnitude:SDATa
Command Syntax
:DISK:DWIZard:LFMagnitude:SDATa {ON | OFF}
Description
When saving a Documentation Wizard zip file (:DISK:DWIZard:SAVE), use this command to add a screen capture of the Log-Freq-Mag plot from the Phase Noise analysis. The file is named Log-Freq-Mag Window Screen Capture.png. The instrument must have the Phase Noise analysis results displayed.
ON- Includes files in Documentation Wizard zip file.
OFF- Excludes files in Documentation Wizard zip file.
Query Syntax
:DISK:DWIZard:LFMagnitude:SDATa?
Query Response
{1 | 0}