:DISK:DWIZard:MHIStogram{1:4}:SDATa
Command Syntax
:DISK:DWIZard:MHIStogram{1:4}:SDATa {ON | OFF}
Description
When saving a Documentation Wizard zip file (:DISK:DWIZard:SAVE), use this command to add the results shown in the Measurement Histogram graph. The data is placed in a comma-delimited ASCII file (Measurement Histogram N Graph Results.csv). A screen capture of the Measurement Histogram graph (Meas Hist N Window Screen Capture.png) is also saved. The instrument must have the Measurement Histogram graph displayed.
ON- Includes files in Documentation Wizard zip file.
OFF- Excludes files in Documentation Wizard zip file.
Query Syntax
:DISK:DWIZard:MHIStogram{1:4}:SDATa?
Query Response
{1 | 0}