:DISK:DWIZard:FPResults{1:64}:SDATa

Command Syntax

:DISK:DWIZard:FPResults{1:64}:SDATa {ON | OFF}

Description

When saving a Documentation Wizard zip file (:DISK:DWIZard:SAVE), use this command to add the results shown in the FFT Peaks results table. The data is placed in a comma-delimited ASCII file (FFT Peaks N Results.csv). A screen capture of the FFT Peaks results table (FFT Peaks N Window Screen Capture.png) is also saved. The instrument must have the FFT Peaks results table displayed.

ON
Includes files in Documentation Wizard zip file.
OFF
Excludes files in Documentation Wizard zip file.

Query Syntax

:DISK:DWIZard:FPResults{1:64}:SDATa?

Query Response

{1 | 0}