:DISK:DWIZard:IRESponse{1:4}:SDATa

Command Syntax

:DISK:DWIZard:IRESponse{1:4}:SDATa {ON | OFF}

Description

When saving a Documentation Wizard zip file (:DISK:DWIZard:SAVE), use this command to add the results shown in the Impulse Response plot. A screen capture of the Impulse Response plot (Impulse Response N Window Screen Capture.png) is saved. The instrument must have the Impulse Response window displayed.

ON
Includes files in Documentation Wizard zip file.
OFF
Excludes files in Documentation Wizard zip file.

Query Syntax

:DISK:DWIZard:IRESponse{1:4}:SDATa?

Query Response

{1 | 0}