:DISK:DWIZard:RESults:SDATa

Command Syntax

:DISK:DWIZard:RESults:SDATa {ON | OFF}

Description

When saving a Documentation Wizard zip file (:DISK:DWIZard:SAVE), use this command to add the results shown in the measurement Results table. The data is placed in a comma-delimited ASCII file (Results Window Results.csv). A screen capture of the Results table (Results Window Screen Capture.png) is also saved. The instrument must have the Results table displayed.

ON
Includes files in Documentation Wizard zip file.
OFF
Excludes files in Documentation Wizard zip file.

Query Syntax

:DISK:DWIZard:RESults:SDATa?

Query Response

{1 | 0}