:DISK:DWIZard:PROTocol{1:4}:SDATa
Command Syntax
:DISK:DWIZard:PROTocol{1:4}:SDATa {ON | OFF}
Description
When saving a Documentation Wizard zip file (:DISK:DWIZard:SAVE), use this command to add the results shown in the Protocol listing window. The data is placed in a comma-delimited ASCII file (Protocol N Results.csv). A screen capture of the Protocol listing window (Protocol N Window Screen Capture.png) is also saved. The instrument must have the Protocol Listing window displayed.
ON- Includes files in Documentation Wizard zip file.
OFF- Excludes files in Documentation Wizard zip file.
Query Syntax
:DISK:DWIZard:PROTocol{1:4}:SDATa?
Query Response
{1 | 0}