:DISK:DWIZard:NOISe{1:4}:SDATa

Command Syntax

:DISK:DWIZard:NOISe{1:4}:SDATa {ON | OFF}

Description

When saving a Documentation Wizard zip file (:DISK:DWIZard:SAVE), use this command to add the results shown in the Noise results window. The data is placed in a comma-delimited ASCII file (Noise N Results.csv). A screen capture of the Noise results window (Noise N Window Screen Capture.png) is also saved. The instrument must have the Noise results window displayed.

ON
Includes files in Documentation Wizard zip file.
OFF
Excludes files in Documentation Wizard zip file.

Query Syntax

:DISK:DWIZard:NOISe{1:4}:SDATa?

Query Response

{1 | 0}