:DISK:DWIZard:MTESt{1:16}:SDATa

Command Syntax

:DISK:DWIZard:MTESt{1:16}:SDATa {ON | OFF}

Description

When saving a Documentation Wizard zip file (:DISK:DWIZard:SAVE), use this command to add the results shown in the Mask test results table. The data is placed in a comma-delimited ASCII file (Mask Test Window Results.csv). A screen capture of the Amplitude results table (Mask Test Window Screen Capture.png) is also saved. The instrument must have the Mask test results displayed.

ON
Includes files in Documentation Wizard zip file.
OFF
Excludes files in Documentation Wizard zip file.

Query Syntax

:DISK:DWIZard:MTES{1:16}t:SDATa?

Query Response

{1 | 0}