:DISK:DWIZard:PNMWindow:SDATa

Command Syntax

:DISK:DWIZard:PNMWindow:SDATa {ON | OFF}

Description

When saving a Documentation Wizard zip file (:DISK:DWIZard:SAVE), use this command to add the results shown in the Phase Noise Markers results window. The data is placed in a comma-delimited ASCII file (Phase Noise Markers Window Results.csv). A screen capture of the results window (Phase Noise Markers Window Screen Capture.png) is also saved. The instrument must have the Phase Noise Markers results window displayed.

ON
Includes files in Documentation Wizard zip file.
OFF
Excludes files in Documentation Wizard zip file.

Query Syntax

:DISK:DWIZard:PNMWindow:SDATa?

Query Response

{1 | 0}