:DISK:DWIZard:MWINdow:SDATa

Command Syntax

:DISK:DWIZard:MWINdow:SDATa {ON | OFF}

Description

When saving a Documentation Wizard zip file (:DISK:DWIZard:SAVE), use this command to add the results shown in the Marker results content window. The data is placed in a comma-delimited ASCII file (Markers Window Results.csv). A screen capture of the Amplitude results table (Markers Window Screen Capture.png) is also saved. Markers must be turned on and the Markers results content window must be displayed.

ON
Includes files in Documentation Wizard zip file.
OFF
Excludes files in Documentation Wizard zip file.

Query Syntax

:DISK:DWIZard:MWINdow:SDATa?

Query Response

{1 | 0}