:DISK:DWIZard:LLTResults:SDATa

Command Syntax

:DISK:DWIZard:LLTResults:SDATa {ON | OFF}

Description

When saving a Documentation Wizard zip file (:DISK:DWIZard:SAVE), use this command to add the results shown in the Limit Lines panel. The data is placed in a comma-delimited ASCII file (Limit Lines Window Results.csv). A screen capture of the Limit Lines panel (Limit Lines Window Screen Capture.png) is also saved.

ON
Includes files in Documentation Wizard zip file.
OFF
Excludes files in Documentation Wizard zip file.

Query Syntax

:DISK:DWIZard:LLTResults:SDATa?

Query Response

{1 | 0}