:DISK:DWIZard:SHERtz{1:4}:SDATa

Command Syntax

:DISK:DWIZard:SHERtz{1:4}:SDATa {ON | OFF}

Description

When saving a Documentation Wizard zip file (:DISK:DWIZard:SAVE), use this command to add an ASCII data file (XY-value waveform file) for each displayed waveform in any Seconds (Hz) waveform content windows. Seconds (Hz) waveform content windows display waveforms from different sources:

  • FFT function. Saves one waveform file for each displayed waveform (example, FFT[1] (F1).txt)
  • S-parameters. Saves one waveform file for each displayed waveform (for example, S11 Delay.txt).

A screen capture each displayed Seconds (Hz) waveform content window is also saved (Seconds (Hz) N Window Screen Capture.png).

ON
Includes files in Documentation Wizard zip file.
OFF
Excludes files in Documentation Wizard zip file.

Query Syntax

:DISK:DWIZard:SHERtz{1:4}:SDATa?

Query Response

{1 | 0}