:DISK:DWIZard:SRESponse{1:4}:SDATa

Command Syntax

:DISK:DWIZard:SRESponse{1:4}:SDATa {ON | OFF}

Description

When saving a Documentation Wizard zip file (:DISK:DWIZard:SAVE), use this command to add the results shown in the Step Response plot. A screen capture of the Step Response plot (Step Response N Window Screen Capture.png) is saved. The instrument must have the Step Response window displayed.

ON
Includes files in Documentation Wizard zip file.
OFF
Excludes files in Documentation Wizard zip file.

Query Syntax

:DISK:DWIZard:SRESponse{1:4}:SDATa?

Query Response

{1 | 0}