:DISK:DWIZard:HRESults{1:4}:SDATa

Command Syntax

:DISK:DWIZard:HRESults{1:4}:SDATa {ON | OFF}

Description

When saving a Documentation Wizard zip file (:DISK:DWIZard:SAVE), use this command to add the results shown in the Waveform Histogram results table. The data is placed in a comma-delimited ASCII file (WHist Stats Window Results.csv). A screen capture of the Waveform Histogram results table (WHist Stats Window Screen Capture.png) is also saved. The instrument must have the Waveform Histogram results table displayed.

ON
Includes files in Documentation Wizard zip file.
OFF
Excludes files in Documentation Wizard zip file.

Query Syntax

:DISK:DWIZard:HRESults{1:4}:SDATa?

Query Response

{1 | 0}