:DISK Documentation Wizard Commands

Configures and saves a Documentation Wizard file (.zip). Use the :DISK:DWIZard:FNAMe command to specify the name of saved file and the :DISK:DWIZard:SAVE command to actually save the file. To select the type of information that is saved in the zip file, use the commands shown in the following table. The files that get saved are listed in the command descriptions.

Commands Used to Select Data to Save
Item Selected with Command Saved in Zip File
:DISK:DWIZard:DBHertz{1:4}:SDATa Decibels (Hz) window data
:DISK:DWIZard:DHERtz{1:4}:SDATa Degrees (Hz) window data
:DISK:DWIZard:ECResults:SDATa Eye Contours results
:DISK:DWIZard:FPResults{1:64}:SDATa FFT Peaks results
:DISK:DWIZard:HRESults{1:4}:SDATa Waveform Histogram results
:DISK:DWIZard:IRESponse{1:4}:SDATa Impulse Response plot
:DISK:DWIZard:JITTer{1:4}:SDATa Jitter results window
:DISK:DWIZard:LFMagnitude:SDATa Log-Freq-Mag plot from Phase Noise analysis
:DISK:DWIZard:LLTResults:SDATa Limit Line Test results
:DISK:DWIZard:MHIStogram{1:4}:SDATa Measurement Histogram results
:DISK:DWIZard:MTESt{1:16}:SDATa Mask Test results
:DISK:DWIZard:NOISe{1:4}:SDATa Noise results window
:DISK:DWIZard:PNMWindow:SDATa Phase Noise Marker results
:DISK:DWIZard:PROTocol{1:4}:SDATa Protocol listing window
:DISK:DWIZard:RESults:SDATa Measurement results
:DISK:DWIZard:SHERtz{1:4}:SDATa Seconds (Hz) window data
:DISK:DWIZard:SRESponse{1:4}:SDATa Step Response plot
:DISK:DWIZard:SSCReen Screen capture of entire display
:DISK:DWIZard:SSETup Instrument setup file
:DISK:DWIZard:SSINfo System information
:DISK:DWIZard:SSParam S-Parameter files
:DISK:DWIZard:TIME{1:4}:SDATa Waveform window data

Example

:DISK:DWIZard:SSCReen ON
:DISK:DWIZard:SSETup ON
:DISK:DWIZard:SSINfo OFF
:DISK:DWIZard:RESults:SDATa ON
:DISK:DWIZard:FNAMe "%USER_DATA_DIR%\Documentation Results\DocumentationResults_PAM4"
:DISK:DWIZard:SAVE
*OPC?