:CHANnel:SIRC:AUPDates
Command Syntax
:CHANnel{1:8}{A|B|C|D}:SIRC:AUPDates
Where the required specifier {1:8}{A|B|C|D} identifies a channel by its module slot number and channel letter. For example, channel 3C (CHANnel3C).
The channel specifier will fail if it does not include a slot number. If instead the suffix's channel letter is missing, the command defaults to letter A. As a result, the best practice is to always explicitly specify the channel by including both the module slot number and channel letter.
Description
Turns on or off automatic updating of SIRC data from a local drive or networked drive. To manually check for updates, use the :CHANnel:SIRC:CFUPdate command. Use the :CHANnel:SIRC:DSTore command to select the location for getting SIRC data files: the local drive. Use the :CHANnel:SIRC:CFOLder command to select the local folder for saving SIRC data files.
Requires an 86105C, 86105D, 86115D, or 86116C module with Option IRC.
Pattern lock must be turned on (:TRIGger:PLOCk) before you can apply SIRC data.
Starting with FlexDCA revision A.07.80, System Impulse Response Correction (SIRC) data files for the 861xxx-series DCA plug-in modules are no longer available for automatic download. To request a SIRC data file for one of these modules, contact Keysight at www.keysight.com/find/keysight care or email support@keysight.com. You will need to supply Keysight with the plug-in module's model and serial number.
Example Command Sequence
:CHANnel2A:SIRC:AUPDates ON