:CHANnel:SIRC:OPResets:SELections?
Query Syntax
:CHANnel{1:8}{A|B|C|D}:SIRC:OPResets:SELections?
Where the required specifier {1:8}{A|B|C|D} identifies a channel by its module slot number and channel letter. For example, channel 3C (CHANnel3C).
The channel specifier will fail if it does not include a slot number. If instead the suffix's channel letter is missing, the command defaults to letter A. As a result, the best practice is to always explicitly specify the channel by including both the module slot number and channel letter.
Query Response
Returns a comma-separated string of available optical SIRC filter presets. For example,
"33 GHz Bessel (Ethernt), 40 GHz Bessel (OIF-CEI)"
Description
For a module that supports optical SIRC filters with presets. Presets are saved bandwidth and rate settings for a SIRC filter. This query returns a comma-separated string of all available presets. Use the CHANnel:SIRC:OPResets command to select a preset.
Requires FlexDCA revision A.06.60 and above.