:CHANnel:SIRC:CFOLder
Command Syntax
:CHANnel{1:8}{A|B|C|D}:SIRC:CFOLder "folder"
"folder" is a string. This command supports the DEFault common child commands.
Where the required specifier {1:8}{A|B|C|D} identifies a channel by its module slot number and channel letter. For example, channel 3C (CHANnel3C).
The channel specifier will fail if it does not include a slot number. If instead the suffix's channel letter is missing, the command defaults to letter A. As a result, the best practice is to always explicitly specify the channel by including both the module slot number and channel letter.
Query Syntax
:CHANnel{1:8}{A|B|C|D}:SIRC:CFOLder?
Description
Selects the local folder for storing the SIRC data files. The default folder is %USER_DATA_DIR%/SIRC Calibrations.
| FlexDCA Running Embedded on N1000A |
N1010A Running on Windows 7 PC |
|---|---|
|
|
Requires an 86105C, 86105D, 86115D, or 86116C module with Option IRC.
Pattern lock must be turned on (:TRIGger:PLOCk) before you can apply SIRC data.