:CHANnel:SIRC:DSTore
Instrument:
N1000A
Flex Apps:
FlexDCA
Package License:
L-RND
Command Syntax
:CHANnel{1:8}{A|B|C|D}:SIRC:DSTore {LDRive | RDCA}
Where the required specifier {1:8}{A|B|C|D} identifies a channel by its module slot number and channel letter. For example, channel 3C (CHANnel3C).
The channel specifier will fail if it does not include a slot number. If instead the suffix's channel letter is missing, the command defaults to letter A. As a result, the best practice is to always explicitly specify the channel by including both the module slot number and channel letter.
Query Syntax
:CHANnel{1:8}{A|B|C|D}:SIRC:DSTore?
Description
Selects the location for loading and updating SIRC data files.
- LDRive
- Load SIRC data from a local folder on a PC.
- RDCA
- Load SIRC data from a local N1000A folder on a remotely controlled N1000A.
- KEYSight (Removed)
- The
KEYSightcommand argument was removed in FlexDCA revision A.07.61 and above and System Impulse Response Correction (SIRC) data files for the 861xxx-series DCA plug-in modules are no longer available for automatic download. To request a SIRC data file for one of these modules, contact Keysight at www.keysight.com/find/keysight care or email support@keysight.com. You will need to supply Keysight with the plug-in module's model and serial number.
Requires an 86105C, 86105D, 86115D, or 86116C module with Option IRC.
Pattern lock must be turned on (:TRIGger:PLOCk) before you can apply SIRC data.
Example Command
:CHANnel2A:SIRC:DSTore LDRive