:CHANnel:SIRC:FBANdwidth
Command Syntax
:CHANnel{1:8}{A|B|C|D}:SIRC:FBANdwidth <bandwidth>
<bandwidth> is a double.
Where the required specifier {1:8}{A|B|C|D} identifies a channel by its module slot number and channel letter. For example, channel 3C (CHANnel3C).
The channel specifier will fail if it does not include a slot number. If instead the suffix's channel letter is missing, the command defaults to letter A. As a result, the best practice is to always explicitly specify the channel by including both the module slot number and channel letter.
Query Syntax
:CHANnel{1:8}{A|B|C|D}:SIRC:FBANdwidth?
Description
SIRC data is created for specific filter rates and 3 dB bandwidths. Once the SIRC data has been loaded, use this command to select the 3 dB bandwidth or use the :CHANnel:SIRC:FRATe command to select the filter rate. Use the :CHANnel:SIRC:DSTore command to load the SIRC data for the module.
Requires an 86105C, 86105D, 86115D, or 86116C module with Option IRC.
Pattern lock must be turned on (:TRIGger:PLOCk) before you can apply SIRC data.