:CHANnel:SIRC:CSTatus:REASon?
Query Syntax
:CHANnel{1:8}{A|B|C|D}:SIRC:CSTatus:REASon?
                                            Where the required specifier {1:8}{A|B|C|D} identifies a channel by its module slot number and channel letter. For example, channel 3C (CHANnel3C).
The channel specifier will fail if it does not include a slot number. If instead the suffix's channel letter is missing, the command defaults to letter A. As a result, the best practice is to always explicitly specify the channel by including both the module slot number and channel letter.
Description
If the SIRC calibration data is ready to use, this query returns the SIRC calibration status, for example  "The SIRC calibration data from 23 October 2011 18:28 GMT is currently loaded.". If the SIRC calibration data is not ready to use, a reason is returned. For example, a very common reason is the lack of pattern lock, which is indicated by the string "You must enable pattern lock to use SIRC." 
Requires an 86105C, 86105D, 86115D, or 86116C module with Option IRC.
Example Command
:CHANnel2A:SIRC:CSTatus:REASon?