:CHANnel:SIRC:USTatus:REASon?
Instrument:
N1000A
N109X
Flex Apps:
FlexDCA
Package License:
L-RND
Query Syntax
:CHANnel{1:8}{A|B|C|D}:SIRC:USTatus:REASon?
Where the required specifier {1:8}{A|B|C|D} identifies a channel by its module slot number and channel letter. For example, channel 3C (CHANnel3C).
The channel specifier will fail if it does not include a slot number. If instead the suffix's channel letter is missing, the command defaults to letter A. As a result, the best practice is to always explicitly specify the channel by including both the module slot number and channel letter.
Description
Queries the reason string associated with the :CHANnel:SIRC:USTatus? query.
Requires an 86105C, 86105D, 86115D, or 86116C module with Option IRC.
Pattern lock must be turned on (:TRIGger:PLOCk) before you can apply SIRC data.
Example Command
:CHANnel2A:SIRC:USTatus:REASon?