:CHANnel:SIRC:OPResets
Command Syntax
:CHANnel{1:8}{A|B|C|D}:SIRC:OPResets "preset"
Where the required specifier {1:8}{A|B|C|D} identifies a channel by its module slot number and channel letter. For example, channel 3C (CHANnel3C).
The channel specifier will fail if it does not include a slot number. If instead the suffix's channel letter is missing, the command defaults to letter A. As a result, the best practice is to always explicitly specify the channel by including both the module slot number and channel letter.
Query Syntax
:CHANnel{1:8}{A|B|C|D}:SIRC:OPResets?
Query Response
Returns a string that identifies the currently selected preset. For example,
"33 GHz Bessel (Ethernt)"
Description
For a module that supports optical SIRC filters with presets. Presets are saved bandwidth and rate settings for a SIRC filter. The command form selects a preset. The query form returns the currently selected preset. To turn on or off the application of channel SIRC, use the :CHANnel:SIRC command.
Requires FlexDCA revision A.06.60 and above.