:CHANnel:SIRC:RESPonse
Command Syntax
:CHANnel{1:8}{A|B|C|D}:SIRC:RESPonse {BESSel | SINC | FLAT}
Where the required specifier {1:8}{A|B|C|D} identifies a channel by its module slot number and channel letter. For example, channel 3C (CHANnel3C).
The channel specifier will fail if it does not include a slot number. If instead the suffix's channel letter is missing, the command defaults to letter A. As a result, the best practice is to always explicitly specify the channel by including both the module slot number and channel letter.
Query Syntax
:CHANnel{1:8}{A|B|C|D}:SIRC:RESPonse?
Description
For a module that has SIRC data for an electrical channel (versus an optical module), selects the filter type. The filter type for optical modules is always a Bessel filter.
- BESSel
- Selects a Bessel filter.
- SINC
- Selects a sinc (Sin(x)/x) filter.
- FLAT
- Selects a flat filter.
Requires an 86105C, 86105D, 86115D, or 86116C module with Option IRC.
Requires FlexDCA revision A.02.00 and above.
Pattern lock must be turned on (:TRIGger:PLOCk) before you can apply SIRC data.
Example Command
:CHANnel2A:SIRC:RESPonse BESSel