:CRECovery:ACDRate?
Instrument:
DCA-X
DCA-M
Meas. mode:
Scope
Eye
Jitter
Flex Apps:
FlexDCA
FlexRT
Query Syntax
:CRECoveryN:ACDRate?
Where N identifies slot number {1:8} which is associated with clock recovery module. On 86108A modules, specify slot 1.
Description
Indicates if the clock recovery module allows continuous (as opposed to discrete) data rate settings. The returned values are:
- 1
- Continuous data rate settings are available.
- 0
- Continuous data rate setting are not available.
Command Compatibility
- N107x-series
- 86108A/B
- 83496A/B