:CRECovery:ELEVel
Instrument:
DCA-X
DCA-M
Meas. mode:
Scope
Eye
Jitter
Flex Apps:
FlexDCA
FlexRT
Command Syntax
:CRECoveryN:ELEVel <integer>
Where N identifies the slot number and must be selected from {1:8}.
Where <integer> is a percentage from 0% to 100%.
Query Syntax
:CRECoveryN:ELEVel?
Query Response
<integer>
Description
Fine tunes the equalization level on the PLL loop characteristics for clock recovery. The default value is 0%. The range can be set from 0% to 100%.
Requires FlexDCA revision A.05.70 and above.