:CRECovery:CFRequency?
Instrument:
DCA-X
DCA-M
Meas. mode:
Scope
Eye
Jitter
Flex Apps:
FlexDCA
FlexRT
Query Syntax
:CRECoveryN:CFRequency?
Where N identifies slot number {1:8} which is associated with clock recovery module. On 86108A modules, specify slot 1.
Query Response
The <clock frequency>, a real number, in Hertz.
Description
Returns the frequency of the recovered data clock an 86108A/B modules.
Command Compatibility
- 86108A/B
Requires FlexDCA revision A.02.00 and above.