:CRECovery:RDIVider
Instrument:
N1000A
DCA-M
Meas. mode:
Scope
Eye
Jitter
Flex Apps:
FlexDCA
FlexRT
Command Syntax
:CRECovery{1:8}:RDIVider <ratio>
<ratio> is an int.
Where the {1:8} specifier identifies a slot number which is associated with clock recovery module. On 86108A modules, specify slot 1.
Query Syntax
:CRECovery{1:8}:RDIVider?
Description
Sets the data-rate divide ratio. This value is used to compute loop bandwidth when the rate-dependent loop bandwidth mode is selected (:CRECovery{1:8}:LBWMode RDEPendent command). Loop bandwidth is set by dividing the data rate (:CRECovery{1:4}CRATe command) by the data-rate divide ratio set with this command. Because the available range of ratios is dependents on the data rate, use the :MINimum and :MAXimum child commands to determine the range.
Command Compatibility
- 86108A/B
- 83496B Option 300
- 83496A Option 300