:CRECovery:ACLBandwidth?
Instrument:
N1000A
DCA-M
Meas. mode:
Scope
Eye
Jitter
Flex Apps:
FlexDCA
FlexRT
Query Syntax
:CRECovery{1:8}:ACLBandwidth?
Where the {1:8} specifier identifies a slot number which is associated with clock recovery module. On 86108A modules, specify slot 1.
Description
Indicates if the clock recovery module allows continuous (as opposed to discrete) loop bandwidth settings. The returned values are:
- 1
- Continuous loop bandwidth settings are available. Use the
:CRECovery<N>:CLBandwidthcommand to set the loop bandwidth. - 0
- Continuous loop bandwidth setting are not available. Use the
:CRECovery<N>:LBANdwidthcommand to select the loop bandwidth.
Command Compatibility
- N107x-series
- 86108A/B
- 83496A/B