:CRECovery:ODRatio:AUTO
Instrument:
N1000A
DCA-M
Meas. mode:
Scope
Eye
Jitter
Flex Apps:
FlexDCA
FlexRT
Command Syntax
:CRECovery{1:8}:ODRatio:AUTO {ON | OFF | 1 | 0}
Where the {1:8} specifier identifies a slot number which is associated with clock recovery module. On 86108A modules, specify slot 1.
Query Syntax
:CRECovery{1:8}:ODRatio:AUTO?
Query Response
{1 | 0}
Description
Enables or disables the automatic selection of the front-panel recovered clock output divide ratio. The output divide ratio is automatically set to 1:1 for frequencies equal to or less than 7.1 GHz or 1:2 for frequencies greater than 7.1 GHz. Use the :CRECovery:ODRatio command to manually set the ratio.
Command Compatibility
- 86108A/B
- 83496B
- 83496A